fp-prysmian

New high capacity under-water cable makes waves

categories: Telecom 

05/06/2015 - 08:14 AM

FirstPath had a requirement – the highest capacity underwater cable possible and Prysmian were

ready.

 

Given the huge expense and complexity of underwater cable deployment, coupled with rising fibre

demand, FirstPath needed a new underwater solution. The cable needed to be small and lightweight

for easy installation but also offer the highest possible fibre capacity.

Prysmian were up to the challenge. Their latest design combines Prysmian’s award-winning

Bendbright-XS fibre with advanced FlexTube cable technology, to create an incredibly fibre dense

underwater cable.

 

"This installation is a major step forward for FirstPath and further expands our network

infrastructure enabling us to tackle the challenges of increasing fibre demand", says FirstPath CEO

Stephen Carter. "The ability to more than double the installed fibre capacity for almost the same

installation cast of the typical 312 fibre underwater cable was a very attractive offering from

Prysmian. Their outside of the box thinking was a perfeet fit for our company’s needs".

 

The installation presents a first for both companies. FirstPath’s first underwater cable deployment

and Prysmian’s highest fibre-count underwater cable. "This innovative approach provides 720 fibre

cores in the same form factor as a conventional 312 fibre solution. This lowers the total cost of

ownership, providing over double the fibre capacity per cable for the same installation costs. This

way we can provide even more value to our customers" says Alice Codenotti, Telecom Account

Manager at Prysmian.

 

Prysmian has Iong been a leader in harbour-crossing cables. This latest offering pushes the

boundaries of cable technology and manufacturing. The project required the collaboration of

multiple R&D centres within Prysmian group. In just six months after initial consultation Prysmian

were able to design, manufacture and deliver a solution to meet FirstPath’s needs. The cable was

installed under the Sydney Harbour Bridge, providing two separate cross-harbour links to add to

FirstPath’s ever growing fibre network.

 

Learn more about our Fibre cables