OUR INNOVATIVE CABLE SOLUTIONS MEET THE NEEDS OF DIVERSE APPLICATIONS
A comprehensive and diversified offering to electrify industry
The electrification of energy end uses is a key pillar of decarbonisation and one of the major efforts required to reach the zero-emission goals set worldwide.
While the global energy demand is expected to remain stable over the next 30 years, the electricity share of the total energy mix is expected to double from 20% to 40% over the same period, mainly because of the shift of fossil fuel-based applications – like gas heating or internal combustion engines - towards electricity, particularly from renewable sources, and because of the growing expansion of electricity-based applications such as data centres.
The more electricity applications grow, the stronger is the demand for a wide-ranging and specialised cable solutions offering in order to meet the needs of the diverse applications and capture the opportunities offered by this market-shaping megatrend.
With our new Connect to Lead business strategy, we aim at seizing the opportunities stemming from the structural megatrends driving the cable market and become a global cable solutions provider leading the energy transition and digital transformation.