Put people before profit
There are A-cables, B-cables and evidently also E-cables. For a second time in a matter of months we hear of hazardous, life threatening cables being sold and installed in Australia! This time it’s Ecables’ copper clad aluminium RE-110 insulated power cables that are being recalled. Its poor insulation can be damaged if exposed to heat above 50°C, risking fire and electric shock. So, stop trying to save nickels and dimes and put people’s safety first.
Choose thoroughly tested A-cables from Prysmian. Australian made? Yes, of course.